AKD Drive

First generation AKD drives support one axis per drive, while AKD2G drives support two axes per drive.
When configuring drives in the EtherCAT Devices tab, you need to designate which motion axis applies to each drive axis, which is the actual axis the drive controls.

In addition to different views, WorkBench provides a WorkBench Toolbar and WorkBench Status Bar to display some extra information.

See WorkBench 2 in the KAS-IDE for more information.

WorkBench Toolbar

The toolbar provides access to these actions:

Figure 3-16: AKD Toolbar


  • To stop all the AKD drives at the same time, click the Stop button in the Device Toolbar.

WorkBench Status Bar

The status bar provides the following information on the drive:

  • A fault indicator (No Faults / x Faults) that becomes red when any AKD gets a fault.
  • The drive status: active / inactive.
  • The software (SW) enable status.
  • The hardware (HW) enable status.

AKD Status Bar

Figure 3-17: AKD Status Bar

For the SW and HW enable status indicators, the color code is:

  • Green when it is OK (i.e., everything is ready to do motion).
  • Red in case of errors / faults.
  • Grey for all other cases (e.g., when SW or HW is not enabled, the status is not green because a motion could not happen, and not red because it is not an error).

Concept Link IconSee Also